|
 |
 |
Products - AT-RTOS32Win - Real-time Virtualization
|

|
|
|
On Time RTOS-32 and Microsoft Windows®
|

|
|
|
AT-RTOS32Win: A member of the KUKA RTOSWin Product Family
The KUKA Virtual Machine Framework together with the underlying RTOS Virtual Machine are a world-wide unique, sophisticated platform for running any arbitrary Real-time Operating System (RTOS) co-existently with Microsoft Windows®. The real-time software may either run with high priority together with Windows on the same CPU core or it may exclusively facilitate one ore more CPU cores. Running different real-time operating systems as well as different instances of the same RTOS on different CPU cores is possible. With AT-RTOS32Win, this platform is now available for On Time RTOS-32 users. Then, for example, the following operation modes are available:
|
|
|
 |
Single-Core CPU: On Time RTOS-32 operates on top of Windows. |
 |
Dual-Core CPU: Windows uses the first core, On Time RTOS-32 uses the second one. |
 |
Quad-Core CPU: Windows uses the first and second core, On Time RTOS-32 uses the third and fourth. |
|
|
|
On Time RTOS-32 (vendor: On Time Informatik GmbH)
|
|
|

|
|
|
Win32 API Compatible Embedded RTOS. On Time's embedded operating system is especially optimized for x86 CPUs, meets hard real-time requirements and implements a Windows subset kernel. It is one of the fastest real-time operating systems on the market running on x86 CPUs. Scheduler performance information can be found here. On Time RTOS-32 can be fully integrated in Microsoft Visual Studio and supports about 290 Win32 API functions. more...
|
|
|
AT-RTOS32Win Software Architecture
|

|
|
|
 |
To execute On Time RTOS-32 under AT-RTOS32Win, On Time RTOS-32 components RTTarget-32 and RTVmf-32 are always required. Most applications will also use RTKernel-32 and the TCP/IP stack RTIP-32. Components RTFiles-32 and RTUSB-32 are also supported. |
 |
On Time Informatik is providing the RTVmf-32 component, the interface for the KUKA RTOS Virtual Machine. |
 |
The RTOS Library provides communication services for On Time RTOS-32 and Windows (e.g. Shared Memory Services, Events to exchange messages and synchronized access on data in the Shared Memory). |
 |
The On Time RTOS-32 binary image, stored on the hard disk, will be started and stopped by the RTOS Uploader Tool. |
|
|
|
AT-RTOS32Win Screen Shot
|
 |
On Time RTOS-32 Debug Monitor was started. |
 |
On Time RTOS-32 messages will be shown in the RTOS-VM Debug Console. |
 |
The Virtual Network Adapter is used as debug interface for On Time RTOS-32. |
 |
Intel PRO/100 Network Adapter is directly controlled by On Time RTOS-32. |
 |
3COM Network Adapter is directly controlled by On Time RTOS-32. |
 |
COM1 Port is also directly controlled by On Time RTOS-32. |
|
|
|

|
|
|
More informationen
|
Data sheets and evaluation versions are available in the download area.
|
|
|
(C) 2008 - All rights reserved |
|
Print this page
|