Feature Packs - EC-Master Options
EtherCAT users expect interoperability as well as a well-defined set of functionality which an EtherCAT MainDevice has to provide.
Not all applications of course have the same requirements and thus, not every MainDevice has to support all features of the EtherCAT technology.
The most general requirements of an EtherCAT MainDevice are covered by the Class A and Class B editions of EC-Master, which fully conform to the respective ETG1500 EtherCAT MainDevice directives.
Additional functionality which may be needed for the broad usage of the EtherCAT technology in controllers, plants and machines are available as well.
These features can be considered to be optional, they are described by Feature Packs in the ETG1500 directive. The Feature Pack describes all mandatory MainDevice functionality for a specific feature, e.g. redundancy. EC-Master covers all such defined feature packs and even provides features beyond the officially defined ones. This page provides an overview of the available feature packs and the respective use case.
Overview
- Split-Frame Processing
- External Synchronization
- Superset-ENI
- Hot Connect
- Cable Redundancy
- MainDevice Redundancy
- EoE Third Party Tool Support Package
- EoE Gateway Tool
- UDP Mailbox Gateway
- Real-time Data Acquisition (DAQ) Library
Feature Pack - Split-Frame Processing
The Split-Frame Processing Feature Pack enables the processing of multiple EtherCAT cyclic tasks in separate application threads. From the application perspective, this makes it possible to structure EtherCAT process data across multiple threads. Therefore, process data that requires different cycle times can be handled accordingly.
Additionally, the processing of acyclic communication can also be outsourced to a separate thread.
For example, a typical application for the Split-Frame Processing Feature Pack would have one tasks for servo drives that requires very fast cycle times, and another task for I / O data that does not need very fast processing or special cycle time requirements.
EC-Engineer makes it easy to create configurations with several EtherCAT cyclic tasks:

The timing of an application utilizing Split-Frame Processing application would look like the following:
- Thread 0 runs with a 250 microsecond cycle time and handles the processing of EtherCAT task 0. This thread also sends out the process data for all other tasks.
- Thread 1 runs with a 500 microsecond cycle time and handles only the processing of EtherCAT task 1.
- Thread Acyc runs with a 1 millisecond cycle time and processes only the acyclic communication and also the Master management tasks.

Feature Pack - External Synchronization
The synchronization of system components or production lines with several EtherCAT Segments can be done with different solutions:
- Synchronization by a bridge device.
Depending on the application the accuracy of the synchronization has different requirements. For the synchronization of two production lines often the accuracy in the range of milliseconds is enough.
However if two or more motion control networks should be synchronized it may be necessary to have the Sync-signals exact at the same time in all devices (e.g. for a network wide commutation information) - that means an accuracy better than a microsecond may be needed.
Within one EtherCAT Segment the Distributed Clocks (DC) mechanism can be used, to synchronize the network devices. DC offers accuracy much better than a microsecond.
The first device that should be synchronized is used as the reference clock for that segment.
The synchronization of several EtherCAT Segments with a high accuracy means that the DC reference clocks in the segments must be adjusted.
The synchronization of two or more EtherCAT segments can be done by a Bridge device as shown in this figure.

The Bridge has two EtherCAT connections (internal two EtherCAT SubDevice Controllers are used). The primary port is connected to the first segment; the secondary port is connected to the second segment. One of the two ports can be configured to be the leading time reference. The Bridge can calculate the time difference and offers the TimeControlValue to the Master. The Master can then adjust the Reference Clock. During startup the two segments can be powered-on at different times. That means that there will be an absolute time difference between the two segments.
To synchronize the Secondary Segment two software algorithms are involved:
- DCX: Synchronize the reference clock to bridge device
- DCM: Synchronize the Master timer to reference clock
Feature Pack - Superset-ENI
The Superset-ENI functionality allows the user to adapt the configuration without generating a new ENI file. The base ENI file contains a superset of all the possible connected SubDevices. According to the use case the application can exclude SubDevices from this superset.
Use case 1 - Optional SubDevices
A possible use case of Superset-ENI is that a configuration contains several optional SubDevices that can be excluded depending on their presence.
| The figure on the right shows a simple Superset network configuration containing all possible SubDevices | ![]() |
| A network scan with this Superset network configuration, will lead to a "bus mismatch", if SubDevice 1002 and 1004 are not present | ![]() |
|
With the FP Superset-ENI the non-existing SubDevices 1002 and 1004 are removed from the configuration during run time which will lead to the resulting valid configuration on the right |
![]() |
Use case 2 - Alternative SubDevices
Another use case of Superset-ENI would be that a configuration contains several different alternatives for a SubDevice at a certain position.
| The network on the right includes one SubDevice which may be of different types | ![]() |
| To realize this, an ENI containing all possible SubDevice definitions is needed, e.g. the two SubDevices 9001 and 9002 | ![]() |
| With the FP Superset-ENI the non-existing SubDevice 9001 is removed from the configuration during run time which will lead to the resulting valid configuration on the right | ![]() |
Feature Pack - Hot Connect
Achieving a maximum flexibility with “Hot Connect”
The concept of “Hot Connect” first of all refers to the connecting and disconnecting of SubDevices in a running (hot) system.
However, this is just one of several possible scenarios.
Much more often it is required to operate the system without a perfect match between the EtherCAT network configuration (ENI file) and the actually connected SubDevices or wiring.
Thus the following additional use cases can be covered (without the need to change the ENI configuration file):
- Setting up a complex control system, while parts of the system are not available, powered-off or disconnected.
- Running a system that consists of mandatory as well as optional devices (e.g. in a test & measurement environment)
- Flexibility within the wiring: SubDevices can be connected to different ports (e.g. analogue to CAN).
In order for “Hot Connect” to be used, no special EtherCAT functionality in the SubDevice is required; in fact, any EtherCAT SubDevice may be a member of a HotConnect group (HC group).
Every HC group just has to be uniquely identifiable, most often this is implemented using DIP switches.
This unique SubDevice address then appears either in the Station Alias Register or at some address location within the SubDevice memory.
Both methods are supported by the EtherCAT Master.
Furthermore, the application may program the station alias address by means of the master (e.g. for first-time system initialization).
All EtherCAT activities required to support HC are automatically handled by the stack in the background. There is no need for the application to interact.
Besides, as soon as a SubDevice is connected or disconnected, the application will be informed by a call-back function (notification).
At any time the application may determine the actually connected SubDevice using the appropriate EC-Master stack API function.
Within the HC feature pack the functionality “Border Close” offers additional security against connecting of SubDevices to an incorrect port.
By activating that function, all EtherCAT ports are closed, except the ports which are permitted by the configuration. Therefore SubDevices which are connected to these ports, are simply ignored and the system continues to run perfectly undisturbed.
In this blog post, we explain how to use Hot Connect.
Feature Pack - Cable Redundancy
Cable redundancy is designed to compensate for the failure of a communication cable section in the EtherCAT system. A ring topology, which normally is operated in both directions, is therefore used. Both branches can nevertheless still be reached if the ring is interrupted at some point.

Description
A second network port is used for ring closure at the EtherCAT master control system. Both cyclic and acyclic frames are sent simultaneously through both ports, and are transported through the system.
In the absence of any fault, all the EtherCAT SubDevices are reached in the forward direction (so called processing direction) from the primary port. This means that they are processed, since the EtherCAT SubDevice Controller (ESC) is only passed through in the forward sense.
When there is no fault, all the EtherCAT SubDevices are reached from the secondary port in the reverse direction - the data in the "redundancy" frame is therefore not changed.
In each case, the EtherCAT frames arrive, possibly modified, at the other port, and are checked by the EtherCAT master. In case of a cable break, both frames are processed - each one on the respective side of the failure. Therefore both frames contain a part of the input data. The master has to combine the data of both frames, and gets one frame with all the input data. The working counters from both frames are added to check for its validity. It is unimportant whether an EtherCAT SubDevice is reached from the primary or redundancy port. The EtherCAT master has to consider that a frame on one side is lost and the other frame returns. To find the matching frame it is useful to mark the frames with an identification or use appropriate mechanism.
The cable redundancy is single-error tolerant, i.e. communication with the SubDevices can continue if the cable is interrupted in one place. When the communication is restored the original communication direction is restored. If the communication is interrupted in more than one place, all connections have to be restored before another fault may occur.
Functionality
In case of cable break all types of EtherCAT communications (process data and mailbox protocols) are be supported without any restrictions.
Handling of the following use cases:
- Normal operation
- Stay operational in case of cable break between two SubDevices
- Stay operational in case of cable break between primary port and first SubDevice
- Stay operational in case of cable break between secondary port and last SubDevice
- Stay operational in case of cable fixed
- Start/Stop (State change) in case of cable break
- Adjustment of Auto Increment address in case of cable break
- Frame loss in case of cable break (partner frame was not received)
Feature Pack - MainDevice Redundancy
In order to increase the availability of the EtherCAT system and provide for failure scenarios, a second fully redundant MainDevice system can be added to the network via acontis' MainDevice Redundancy feature. This new feature will create an ACTIVE MainDevice and an INACTIVE Backup MainDevice. In normal operation the INACTIVE Backup MainDevice simply forwards frames through and back onto the network using acontis' optimized Ethernet drivers for fast packet forwarding:

Data Synchronization and Inter-MainDevice Communication
The ACTIVE MainDevice cyclically sends and receives frames to control the EtherCAT SubDevices. The INACTIVE MainDevice acts as a forwarding device.
Furthermore, the MainDevices communicate with each other by sending dedicated EtherCAT frames on the EtherCAT network that are only processed by the other MainDevice, not by the SubDevices. This inter-MainDevice communication is used to synchronize state information from the ACTIVE to the INACTIVE MainDevice and it provides a channel for the applications at the MainDevices to communicate with each other using cyclic and acyclic data.
Failover
If the ACTIVE MainDevice fails, the INACTIVE Backup MainDevice can takeover and become ACTIVE. Due to the fact that the INACTIVE Backup MainDevice has been connected to the network the whole time, it can control the bus after getting ACTIVE in the case of a failover:

Cable Redundancy with MainDevice Redundancy
Cable Redundancy can be combined with MainDevice Redundancy. The ACTIVE MainDevice communicates directly to one segment of the EtherCAT network and indirectly to the other segment of the EtherCAT network through the INACTIVE Backup MainDevice:

Feature Pack - EoE Third Party Tool Support Package
Using the mailbox protocol Ethernet over EtherCAT (EoE) standard Ethernet frames can be tunneled trough an EtherCAT network. Based on this, a communication to SubDevices with locally running TCP/IP-based applications (e.g. Web Server) can be established. More and more manufacturers of EtherCAT drives are supported this connection in their drive setup and tuning tools.
Acontis is offering all required software modules to enable TCP communication between a third party software on Windows and a EtherCAT SubDevice supporting EoE. On the master controller just the proven RAS-Server has to be enabled. The RAS-Server is included in the EC-Master core license and available on many operating systems.
acontis EoE Gateway Tool for Windows
Many EtherCAT products available on the market today offer support for Ethernet over EtherCAT (EoE). EoE provides a convenient way to setup and configure an EtherCAT device without the need to implement a full EtherCAT network. Many manufacturers of EoE-capable EtherCAT devices offer a software tool for setting up and configuring their products. Some examples include: Bosch Rexroth IndraWorks, Yaskawa SigmaWin+, Elmo Application Studio, and Copley CME2.
For developers and users of acontis’ EtherCAT Master software, EC-Master, the convenience of these manufacturer tools is lost by having to disconnect the master controller running EC-Master from the network in order to connect a Windows computer running the software tool directly to the EtherCAT device. Then after some simple changes via the manufacturer tool, the master controller needs to be reconnected again. To address this issue, acontis has released their EoE Gateway Tool for Windows.
With the EoE Gateway tool, acontis provides a convenient way to keep the master controller connected to the EtherCAT devices, but still utilize the manufacturer’s tool for setup and configuration. This is achieved by tunneling the Ethernet data from the tool through the master controller running EC-Master and onto the EtherCAT network.

This EoE Gateway Tool runs in the Windows System Tray in the background so you can focus on the manufacturer tool like it was directly connected to the EtherCAT device.


Feature Pack - UDP Mailbox Gateway
The Mailbox Gateway functionality within a MainDevice can be used to route the EtherCAT mailbox protocol from an (external) device configuration tool via the Mailbox Gateway to the EtherCAT devices and vice versa. All Mailbox protocols that are defined in the EtherCAT specification can be used in general, i.e. CoE, FoE, VoE, SoE.
There is no error handling specified for the Mailbox Gateway functionality. A request to a non-existing SubDevice can lead to no response from the MainDevice. According to Function Guideline „ ETG.8200 EtherCAT Mailbox Gateway“.
Mailbox Gateway Structure

Feature Pack - Real-time Data Acquisition (DAQ) Library
With the Real-time Data Acquisition Library it is possible to record data for different use cases. Normal standard loggers are not real-time and only suitable for a long-term protocol. Also the sample rates are really slow, e.g. 1 second. With the Real-time Data Acquisition Library the sample rates may be as fast as the EtherCAT communication cycle. It is really reliable and deterministic. It is possible to acquire process data variables, application variables and other diagnostic information, e.g. error counters.
Use Cases
- Commissioning, e.g. optimize controller settings
- Troubleshooting, e.g. determine bad cables or connectors
- Condition monitoring, predictive maintenance, e.g. vibration analysis
- Quality assurance, e.g. compare production results with specification
- Documentation, e.g. store production parameters for each produced part
- Real-time data acquisition Recorder (RC) with many options: Sample Rate, Trigger Conditions, etc.
- Store EC-Master process data and application variables in Record File
- Use standardized file formats: MDF4 or CSV
- Use third party tools to evaluate the data
- Use data analysis tools (e.g. cloud analytics to find correlated data)
Features
- Supported output file formats: MDF4, CSV
- Settable limits for output file: Maximal size, Maximal duration
- Support for multiple recorder instances
- store data into multiple files in parallel
- Different settings for each such recorder (e.g. sample rate, trigger conditions)
- Configure recorder instances via API or XML file
- Acquisition of EtherCAT Process Data
- Select specific variables by name
- Select all variables of specific SubDevice by station address
- Select all variables within a specific range (offset and length)
- Acquisition of Application Variables
- Select specific variables by name
- Settable trigger conditions to start and stop recorders