Understanding Real-time Hypervisors: Revolutionizing Industrial Computing

In the rapidly evolving landscape of industrial computing, the advent of Real-time Hypervisors represents a significant leap forward. This cutting-edge technology offers a robust solution to consolidate multiple applications, previously running on separate hardware, onto a single Industrial PC. But what exactly is a Real-time Hypervisor, and how does it transform the industrial computing paradigm?

The Essence of Real-time Hypervisors

A Real-time Hypervisor is a type of virtualization technology designed specifically for use in systems where timing and deterministic performance are critical. Unlike traditional Hypervisors, which focus on maximizing resource utilization and flexibility, Real-time Hypervisors prioritize maintaining the deterministic performance of Real-time operating systems (RTOS) alongside general-purpose operating systems like Windows, Ubuntu, or Debian.

Key Features and Benefits

  • Consolidation of Multiple Applications: Real-time Hypervisors enable the consolidation of various applications running on different hardware into a single Industrial PC. This not only reduces hardware costs but also simplifies system architecture and maintenance.
  • Support for Off-the-shelf Operating Systems: They allow for the running of unmodified versions of popular operating systems such as Windows, Ubuntu, and Debian. This means that industrial setups can leverage the vast ecosystem of existing software and applications without needing specialized versions.
  • Real-time Operating System Performance: One of the core strengths of Real-time Hypervisors is their ability to run RTOS and preserve their deterministic, hard Real-time performance. This is crucial for applications where timing and immediate response are non-negotiable, such as in motion control or Real-time measurement.
  • Enhanced Security through Virtualization: By using virtualization technology to create "air-gaps" between different guest operating systems, Real-time Hypervisors enhance system security. This separation achieves the same effect as utilizing different hardware for each application, safeguarding against cross-contamination or cyber-attacks targeting one part of the system.
  • Broad Industrial Application Support: Real-time Hypervisors are adept at supporting a wide range of typical industrial use cases. These include human interfaces, graphical user interfaces, programmable logic control (PLC), motion control, Real-time measurement, and more advanced applications like machine learning and artificial intelligence, system monitoring, and cloud connection. This versatility makes them an invaluable asset in modern industrial setups.

Transforming Industrial Computing

The adoption of Real-time Hypervisors in industrial computing offers a plethora of advantages. By consolidating hardware and ensuring the safe, efficient operation of multiple operating systems and applications on a single platform, industries can achieve higher levels of performance and security. This is particularly relevant in the era of Industry 4.0, where connectivity, data analysis, and automation play pivotal roles in manufacturing and production processes.

Moreover, the ability to run a mix of Real-time and general-purpose operating systems side by side without sacrificing performance or security opens up new avenues for innovation and efficiency. From enhancing human-machine interfaces to facilitating sophisticated control and monitoring systems, Real-time Hypervisors stand at the forefront of industrial computing evolution.

In conclusion, as industries continue to seek more efficient, secure, and flexible computing solutions, the role of Real-time Hypervisors is set to grow. Their ability to meet the demanding requirements of modern industrial applications while offering the benefits of virtualization technology makes them a cornerstone of next-generation industrial computing infrastructure.

Stay Up to Date