Understanding EtherCAT ENI Files
An EtherCAT Network Information (ENI) file is a standardized XML-based document that provides the necessary configuration data for an EtherCAT MainDevice. It defines the network topology, communication settings, and synchronization parameters, allowing the MainDevice to control and communicate with all connected SubDevices effectively.
The ENI file is typically generated by an EtherCAT configuration tool, such as acontis’ EC-Engineer, based on the ESI (EtherCAT SubDevice Information) files of all SubDevices in the network. Once created, the ENI file is loaded into the EtherCAT MainDevice, enabling it to bring the network online and execute real-time data exchange.
Key Information Contained in an ENI File
An ENI file includes critical configuration details, such as:
- Network Topology – Defines the physical and logical arrangement of all EtherCAT SubDevices.
- Process Data Configuration – Specifies input and output data mapping for each SubDevice.
- Cycle Timing and Synchronization – Configures communication cycles and real-time synchronization settings.
- Mailbox Protocols – Lists supported communication protocols like CoE (CANopen over EtherCAT) or FoE (File over EtherCAT).
- Device-Specific Parameters – Includes individual SubDevice settings, such as operational modes and safety parameters.

How Are ENI Files Used?
When deploying an EtherCAT network, the ENI file plays a crucial role in initializing and maintaining communication between the MainDevice and SubDevices. Here’s how it is used:
1. Generating the ENI File:
The user configures the network within an EtherCAT configuration tool, such as EC-Engineer, which compiles the details of all SubDevices using their respective ESI files. The tool then generates the ENI file, defining the complete network setup.
2. Loading the ENI File into the MainDevice:
The ENI file is transferred to the EtherCAT MainDevice Software Stack, such as EC-Master, which uses it to configure communication with the SubDevices.
3. Initializing the Network:
The EtherCAT MainDevice Software Stack processes the ENI file to establish the network structure, set communication parameters, and prepare for data exchange.
4. Bringing the Network to Operational State:
The EtherCAT MainDevice Software Stack transitions the network through different EtherCAT states, including Initialization, Pre-Operational, Safe-Operational, and Operational, to enable real-time communication and control.

Why Are ENI Files Important?
ENI files enable efficient and reliable EtherCAT network operation by:
- Defining network topology, providing the MainDevice with a detailed description of all connected SubDevices.
- Ensuring real-time communication by configuring synchronization and timing for deterministic EtherCAT performance.
- Automating device configuration, eliminating manual setup by predefining communication parameters.
- Supporting standardized protocols to enable seamless integration of devices from different manufacturers.
Where Can You Find or Generate ENI Files?
Unlike ESI files, which are provided by manufacturers, ENI files are user-generated by EtherCAT configuration software. When creating an ENI file, it’s essential to ensure all ESI files are available and up-to-date, verify network topology accuracy, and test configuration before deployment using EtherCAT diagnostic tools to ensure proper operation.

Key Takeaways
ENI files are fundamental to EtherCAT network operation. They define network topology, configure communication settings, and enable seamless data exchange between MainDevices and SubDevices. By properly generating and validating an ENI file, engineers can ensure robust and efficient EtherCAT network performance.
For more information on EtherCAT networks and ENI files, please contact us or explore the resources on our website.