Programming the EC-Master Core Library in C/C++
EC-Master Core Library and the Remote Access Service (RAS) Server Module are implemented in C++. The API interfaces are C language interfaces, thus the EC-Master can be used in ANSI-C as well as in C++ environments.
- EcMasterDemo is the basic example application for EC-Master. The example shows how to initialize EC-Master and how to put the network into operational state. Based on the provided ENI file this example can handle all kind of EtherCAT SubDevices.
- EcMasterDemoSyncSm demonstrates a different network timing which requires the interrupt from the Ethernet Controller used by EC-Master. This cyclic frame is transmitted at the begin of the cycle and the process data are updated immediately after the frame returns.
- EcMasterDemoDc is a good starting point for application requiring the accurate synchronization of SubDevices based on the Distributed Clocks (DC) technology. To synchronize the MainDevice with the SubDevices several modes can be selected.
- EcMasterDemoMotion comes with a simple motion control library to control drives implemented according to the profile CiA402 and the ETG Implementation Directive ETG.6010. The example supports the operation modes Cyclic Synchronous Position (CSP) and Cyclic Synchronous Velocity (CSV).
Programming the RAS-Client Library in C/C++
The RAS Client Library is part of the Feature Pack Remote Access Service SDK and provides in conjunction the RAS Server the EC-Master programming interface on a remote system. The RAS protocol is by default transported with TCP/IP and Ethernet, but also another infrastructure, e.g., shared memory, can be used.
- The EcMasterDemoRasClient example application demonstrates how to connect to the RAS Server and to call EC-Master APIs like emScanBus or emGetMasterState, access process data using emGetProcessDataBits or send notifications to the EC-Master application.
Operating systems and tools
- Supported Operating Systems: All
- Supported Compilers: Microsoft, GNU, LLVM
- Supported IDE: Microsoft Visual Studio, Eclipse, WindRiver Workbench, QNX Momentics, IAR, Keil MDK
Programming in C#
The example EcMasterDemoDotNet and the .NET wrapper are written in C#. The target platform is AnyCPU. The other libraries are written in C++ and are platform specific. The Wrapper Library is a helper that prepares the API for .NET. The demo runs with MS .NET Framework as well as with Mono.
- EcMasterDemoDotNet is a basic Windows Forms (C#) GUI application for EC-Master. The example shows how to initialize EC-Master and how to put the network into operational state. Based on the provided ENI file this example can handle all kind of EtherCAT SubDevices. It is also shown how to read and write a variable. Even an example of how to read a register from the CoE object dicitionary can be found.
Operating systems and tools
- Supported Operating Systems: Windows (MS .NET 2.0, MS .NET Standard 2.0), Linux (MS .NET Standard 2.0, Mono)
- Supported IDE: Microsoft Visual Studio (Code)
- Supported Compiler: Microsoft
Programming in Python
The examples and the Python wrapper are written in Python. They are not platform specific. The other libraries are written in C++ and are platform specific. The EcWrapper is a helper that prepares the API for python.
- Similar to the other demos the EcMasterDemoPython shows how to call the EC-Master API. There is also a Python demo for the EC-Simulator. The python demos can also run in interactive mode e.g. to set an output of the EtherCAT network or something else. This is very useful to quickly test different behaviors of the EtherCAT network e.g. with the EC-Simulator.
Operating systems and tools
- Supported Operating Systems: Windows (Python 3.7), Linux (Python 3.7)
- Supported IDE: Python IDLE Shell, Microsoft Visual Studio Code
Note: Python Wrapper and SDK is available as additional package not included in the EC-Master Core SDK.
Programming in Rust
Rust is a systems programming language developed by Mozilla Research (released 2015), designed for performance-critical software with strong safety guarantees — giving you the speed of C/C++ without the common pitfalls. The examples and the Rust wrapper are written in Rust. They are not platform specific. The other libraries are written in C++ and are platform specific. The EcWrapper is a helper that prepares the API for python.
- Similar to other demos, the EcMasterDemoRust shows how to call the EC-Master API. There is also a Rust demo for the EC-Simulator available. The Rust demos can also run in interactive mode e. g. to set an output of the EtherCAT network or something else. This is very useful to quickly test different behaviors of the EtherCAT network e. g. with the EC-Simulator.
Operating systems and tools
- Supported Operating Systems: Windows and Linux (Rust v1.90.0 or above)
- Supported IDE: Microsoft Visual Studio Code
Note: RUST Wrapper and SDK is available as additional package and not included in the EC-Master Core SDK.