Introduction to EtherCAT Technology and the EtherCAT Protocol

1 What is EtherCAT?

EtherCAT® (Ethernet for Control Automation Technology) is a real-time Ethernet Fieldbus used in industrial automation, motion control, robotics, test and measurement, and factory automation. It is based on the IEEE 802.3 Ethernet standard and optimized for fast, deterministic cyclic data exchange.
EtherCAT uses a MainDevice/SubDevice architecture: an EtherCAT MainDevice, such as acontis' EC-Master, sends commands and process data to SubDevices such as drives, I/O modules, sensors, and actuators, and receives their data in return. Thanks to EtherCAT’s “on-the-fly” processing, a single frame can be used to exchange data with many devices in one cycle.
The technology was introduced by Beckhoff Automation and is now maintained as an open standard by the EtherCAT Technology Group. Thousands of vendors provide compatible hardware and software, making EtherCAT a widely available and cost-effective choice.
Key benefits of EtherCAT include:
      • Very short, deterministic cycle times suitable for hard real-time control
      • High bandwidth utilization due to on-the-fly frame processing
      • Flexible network topologies (line, tree, star) without external switches
      • Support for Distributed Clocks for precise synchronization across devices

 

Interested in implementing EtherCAT in your system?
Learn more about software options for EtherCAT MainDevices, network configuration, and diagnostics tools.

2 The EtherCAT Protocol Fundamentals

2.1 Frame Structure

As with standard Ethernet communication, EtherCAT utilizes Ethernet frames to transmit data throughout the network. EtherCAT frames are based on the IEEE 802.3 Ethernet standard; however, they are structured in a special way that optimizes them for increased bandwidth and short cyclic process data. EtherCAT frames also eliminate bulkier protocol stacks such as UDP/IP or TCP/IP, meaning that EtherCAT is not an IP-based protocol, more similar to a Layer 2 or Data Link Layer protocol.

The EtherCAT frame, or telegram, consists of an Ethernet header, followed by the EtherCAT data, and is ended by a frame check sequence (FCS). The EtherCAT protocol is identified by using the 0x88A4 identifier in the EtherType field within the Ethernet header. Wireshark contains a dissector to graphically analyze EtherCAT frames.

The EtherCAT data contains an EtherCAT-specific header followed by the EtherCAT Datagrams. The EtherCAT header specifies the total length and type of the subsequent EtherCAT datagrams. Following the EtherCAT header is the EtherCAT datagram, which contains the actual data that is going to be read or written in the network. This data includes address specifications, the command type (i.e. read, write, or read-write) that the MainDevice would like to execute, and the cyclic process data (PDOs). A single EtherCAT frame may contain up to 1,498 bytes.

If more than 1,498 bytes are required, the MainDevice will send out multiple frames of data, and each frame will contain identifiers signaling whether devices on the network should expect another frame behind the current one.

The EtherCAT MainDevice is responsible for assembling the EtherCAT frames and sending them through the network. Every frame sent out by the MainDevice will pass through each node in the network (logical ring). Additionally, thanks to flexible topology options, there is no need for network switches or routers, further reducing timing delays and hardware costs.

2.2 Functional Principle

Along with the frame structure, EtherCAT further differentiates itself with its unique method of exchanging data on the network. Many other Ethernet-based protocols require a separate frame to be sent to each node on the network—and require a response from every node in the network—in each cycle resulting in high network traffic and longer cycle times. Additionally, since each frame only contains data for one node, bandwidth utilization is usually very low and inefficient.

EtherCAT utilizes “on the fly” processing, which allows just one frame to be sent to all nodes. The EtherCAT MainDevice controller assembles the frames and sends them out. In each cycle, the frame travels around the network, passing through each node before returning to the MainDevice. The frames contain information for the SubDevice nodes including addressing, EtherCAT command type (read, write, or read-write), and the actual process data. As each frame travels around the network, each device will look for and extract the data that is addressed to it and insert new data back into the frame all while it travels downstream. When the frame reaches the last node in the network, the frame is sent back to the MainDevice using the full duplex capability of Ethernet.

EtherCAT’s on-the-fly processing provides many performance and cost-saving benefits. For example, although multiple frames can be used in the case of very large networks, a single frame is typically sufficient to send and receive data to and from all nodes. Furthermore, the EtherCAT MainDevice is the only one allowed to send new frames. All other devices on the network simply receive the frame, process the frame, and forward it on. This eliminates unexpected delays and makes EtherCAT suitable for real-time applications.

2.3 Topology

EtherCAT technology offers flexible network topology options, making it a great choice for large and complex networks. EtherCAT networks contain a MainDevice that is controlling the network and subsequent SubDevices. The SubDevices typically have two or more ports that allow them to be connected together.  Network topology possibilities include line, tree, star—or any combination thereof. Since EtherCAT operates in full duplex mode—taking advantage of the line pair in bidirectional Ethernet cables—any topology can maintain a logical ring structure, meaning the frame will always be able to get back to the MainDevice once it is sent out. This flexibility also eliminates the need for network switches.

EtherCAT also supports advanced topology features such as Hot Connect and Hot Swap, meaning devices can be changed, added, or removed from the network all while remaining in the operational state. EtherCAT also supports several redundancy options including cable redundancy and MainDevice redundancy, adding extra protection against line breaks and device failures, further reducing downtime and maintenance costs.

2.4 Process Data

In each cycle, the EtherCAT MainDevice assembles data into the frame and sends it out to the nodes in the network. The nodes read the data addressed to them and write new return data into the frame as it travels downstream. Once the frame reaches the end of the network and returns to the MainDevice, the MainDevice will read the new data, and build the next frame. This data exchanged between the MainDevice and SubDevices is known as cyclic process data.

The SubDevices—using their Fieldbus Memory Management Units (FMMU)—are responsible for reading and writing their data to the correct location in the frame. This is known as data mapping and is essential to ensure that the EtherCAT MainDevice receives a completely sorted process image each cycle. The cyclic process data can be assembled according to project needs by activating optional process data objects. Organizing the process data this way enables EtherCAT’s fast and reliable performance.

Different SubDevice types may have different hardware and process data layout options. For example, simple devices, such as digital I/O, have fixed hardware and fixed process data layouts. Complex devices, such as drives, have fixed hardware and variable process data layout. Furthermore, modular devices, such as bus couplers or gateways, have variable hardware and variable process data layout.

2.5 Communication Profiles and Mailbox Protocols

In addition to cyclic process data, EtherCAT also supports acyclic communication including various mailbox protocols. These EtherCAT communication profiles were established to provide support for a wider variety of field devices and application layers. According to the EtherCAT specification, SubDevices are not required to support all communication profiles; instead, they may support whichever profile or profiles are most suitable and relevant for their use case. Furthermore, in contrast to cyclic process data, mailbox protocol data transfers are not guaranteed to be delivered in any real-time constraint.

2.5.1 CAN Application Protocol over EtherCAT (CoE)

CANopen® is a popular communication protocol for embedded systems often used in automation applications. The EtherCAT communication profile known as CoE allows the implementation of the CAN Application Protocol over an EtherCAT network. This includes support for the CANopen object dictionary, mapping of Process Data Objects (PDOs), CoE Emergency error messages, diagnostics, and Service Data Objects (SDOs). Furthermore, many standardized CANopen profiles, such as the CiA 402 profile for drives and the CiA 406 profile for encoders, can be reused for EtherCAT communication. CoE is often utilized when project-specific parameters are sent to the SubDevice upon startup according to the network configuration. SubDevice parameters can also be inspected and modified while the network is in the operational state via CoE.

2.5.2 Ethernet over EtherCAT (EoE)

Another powerful communication profile is Ethernet over EtherCAT. With EoE, Ethernet data traffic can be transmitted within an EtherCAT network. Switchport devices can be used in the EtherCAT segment to connect to Ethernet devices such as computers and routers. The switchport device is responsible for inserting the TCP/IP fragments into the EtherCAT traffic. EoE is commonly used to access a SubDevice’s web server for device configuration and diagnostics. In this way, the devices appear as if they are connected directly to a non-EtherCAT local network.

2.5.3 File Access over EtherCAT (FoE)

File Access over EtherCAT, or FoE, is another popular mailbox protocol used in EtherCAT communication. FoE is typically used to update firmware to devices in an EtherCAT network.

2.6 Synchronization (Sync Managers and Distributed Clocks)

Synchronization in EtherCAT communication makes real-time performance possible and enables precise and coordinated processes which are common in complex and critical applications. Synchronization guarantees that all nodes in the EtherCAT network are working with the same time base. For example, in high-speed motion control applications, it is critical to have all motor drives receiving and sending commands at the exact same time to ensure that the movements are executed quickly and accurately.

The most precise EtherCAT synchronization mechanism is based on Distributed Clocks (DC), and the calibration of the clocks across nodes in the network is based on hardware. EtherCAT utilizes a reference clock, typically from the first DC SubDevice in the network. The time from this reference clock is distributed throughout all nodes in the network, and the resulting jitter is less than one microsecond. To compensate for the various clock drifts due to speed differences of each clock in the network, the devices regularly adjust themselves according to the reference clock. With all nodes operating on the same reference clock, the process data and output signals can be applied simultaneously across the network using a periodic trigger which is managed by the precise local clock.


3 EtherCAT Implementation

3.1 System Architecture

The system architecture of an EtherCAT implementation can be broken down into three main components: configuration files, the EtherCAT MainDevice, and the EtherCAT SubDevices.  EtherCAT configuration files are used by the MainDevice to configure and initialize an EtherCAT network. The configuration files contain detailed information about the SubDevice configuration and network topology. The MainDevice, also known as the EtherCAT MainDevice, is responsible for managing the EtherCAT network, exchanging data with the SubDevices, and interfacing with outside applications. The SubDevices, known as the EtherCAT SubDevices, are typically sensors, drives, actuators, and simple digital/analog I/O, that perform specific tasks in the automation system.

3.2 EtherCAT SubDevice Information (ESI)

An ESI file, or "EtherCAT SubDevice Information" file, is a type of configuration file used in EtherCAT systems to describe the functionality and configuration settings of EtherCAT SubDevices. ESI files, which are XML based, are provided by the manufacturer or vendor of the SubDevice, and they contain information necessary for the MainDevice to configure and communicate with the SubDevice. The ESI file contains detailed information about the EtherCAT SubDevice, including its device type, its supported mailbox protocols, synchronization settings, and the mapping of its input and output process data (PDO). The SubDevice may contain service data objects (SDOs) and list them in an Object Dictionary. When including the Object Dictionary, the ESI file then includes the complete list of objects.

3.3 EtherCAT Network Information (ENI)

An ENI file, or "EtherCAT Network Information" file, is a type of standardized configuration file used in EtherCAT systems to define the network topology, positioning of the SubDevices in the network, and the process data structures of all EtherCAT SubDevices. The ENI file is typically built using an EtherCAT configuration tool that has defined the network topology (either by scanning the network for EtherCAT SubDevices, or by manually adding SubDevices) and parses the information from the provided ESI files from each SubDevice. The ENI file is used by the EtherCAT MainDevice to configure and initialize the network, and it contains all the necessary information for the MainDevice to communicate with each device on the network.

3.4 MainDevice

An EtherCAT MainDevice, such as acontis' EC-Master, is a device that manages and controls an EtherCAT network. It is typically a PC or embedded microprocessor, a programmable logic controller (PLC), or a motion controller that is responsible for communicating with and controlling the EtherCAT SubDevices that are the devices connected to the network. The EtherCAT MainDevice acts as the point of control for the network, and it is responsible for managing the communication between the SubDevices, issuing commands to the SubDevices, and receiving data from the SubDevices.

The MainDevice is also responsible for managing the network clock and synchronization across the network, and for error-handling mechanisms such as watchdog timers and automatic retries. It also uses the information from the ENI and ESI files to configure the network and to understand the network topology and SubDevice capabilities.

3.5 SubDevice

An EtherCAT SubDevice is a device that is connected to an EtherCAT network and controlled by an EtherCAT MainDevice. These devices are typically sensors, drives, actuators, or other types of automation devices that perform specific tasks in the automation system. In order to enable EtherCAT’s unique on-the-fly frame processing, EtherCAT SubDevices require an EtherCAT SubDevice Controller (ESC). The ESC can be a dedicated chip like an ASIC, implemented as an IP Core in an FPGA, or even integrated directly into the processor. ESCs can be designed manually but are also widely available off-the-shelf from many different manufacturers.

EtherCAT SubDevices communicate with the MainDevice by reading data from and writing data into the EtherCAT frames sent from the MainDevice as they move through the network, and they are also able to communicate with other SubDevices on the network via SubDevice-to-SubDevice communication. Each SubDevice is automatically assigned a unique identification number called an "address", and the MainDevice uses this address to communicate with the SubDevice. The functionality of a SubDevice is defined by the SubDevice's ESI file which is typically provided by the SubDevice’s manufacturer. The ESC allows various topologies and enables cable and MainDevice redundancy.

The SubDevices also have built-in error handling mechanisms, such as watchdog timers and automatic retries, which help to ensure reliable communication and prevent errors from causing the system to fail.

3.6 Error Detection and Diagnosis

EtherCAT has many useful and convenient error detection and diagnostic features built in that make troubleshooting and maintenance fast and easy. Error detection and diagnostics play a major role in determining a machine’s availability, operability, and commissioning time. acontis offers a comprehensive suite of EtherCAT monitoring and diagnostic tools to make troubleshooting EtherCAT networks straightforward.

EtherCAT includes the ability to scan and compare the actual network topology with the configured topology during boot-up. This comparison is useful in detecting cabling issues and other physical layer problems and is an enormous advantage in comparison to conventional fieldbus systems.

Furthermore, with EtherCAT it is possible to determine the exact node in the network where the error was initiated. This is known as error localization. EtherCAT can detect and localize occasional disturbances before the issue impacts the machine’s operation.

The EtherCAT SubDevice Controller in each node checks the moving frame for errors with a checksum. Information is provided to the SubDevice application only if the frame has been received correctly. If there is a bit error, the error counter is incremented and the subsequent nodes are informed that the frame contains an error. The MainDevice will also detect that the frame is faulty and discard its information. The MainDevice can detect where the fault originally occurred in the system by analyzing the nodes’ error counters.

Within the frames, the Working Counter enables the information in each Datagram to be monitored for consistency. Every node that is addressed by the Datagram and whose memory is accessible increments the Working Counter automatically. The MainDevice is then able to cyclically confirm if all nodes are working with consistent data. If the Working Counter has a different value than it should, the MainDevice notifies the application about the discrepancy. The MainDevice is then able to automatically detect the reason for the unexpected behavior with help from status and error information from the nodes as well as the Link Status.

Thanks to EtherCAT’s unique principle of bandwidth utilization, which is orders of magnitude better than industrial Ethernet technologies that use single frames, the likelihood of disturbances induced by bit errors within an EtherCAT frame is substantially lower – if the same cycle time is used. If much shorter cycle times are used, the time required for error recovery is significantly reduced. Thus, it is also much simpler to address such issues within the application.

Since EtherCAT utilizes standard Ethernet frames, Ethernet network traffic can be recorded with the help of free Ethernet software tools. For example, the well-known Wireshark software comes with a protocol interpreter for EtherCAT, so that protocol-specific information, such as the Working Counter, commandos, etc. are shown in plain text.

 

Free Evaluation Request