Technology Partners / Software
Since 1998 AXEL was involved in the production and implementation of embedded software for the industrial automation.
AXEL's experience has increased more and more and thanks to its deep knowledge, AXEL can give to its customers' products the added value which is nowadays represented by software components. www.axelsoftware.it
ISIT provides in-house developed, SIL 3 pre-certified "on demand" FSoE communication stacks, ensuring robust safety for industrial EtherCAT networks.
Compliant with IEC 61784-3-12, our MainInstance/SubInstance solutions guarantee seamless integration and interoperability. The unique architecture allows effortless migration between non-safety and safety versions, streamlining development for diverse applications.
Discover how our FSoE stacks deliver dependable and efficient safety communication. Explore the possibilities for your next industrial project. ISIT FSOE Stack
Neuron Automation is the engineering house for functionally safe automation solutions for component manufacturers. Our aim: to revolutionize functional safety in industrial automation. With smart, modular technologies, we make safety development faster and more cost-efficient. We offer ready-to-use technologies and development services for functional safety, from hardware to firmware, configuration and programming. These include a pre-certified safety toolkit (IEC 61508, ISO 13849) with ready-to-use hardware platforms, software-based safety, and a modern engineering tool with AI-supported, requirement-based code and test generation. For EtherCAT systems, Neuron provides a compact FSoE Host/Device Stack that integrates into existing EtherCAT architectures with little effort. Formed in 2019 through the merger of logi.cals (AT) and ISH Ingenieursozietät (DE), Neuron brings more than 40 years of safety experience. Locations: St. Pölten and Kreuztal.
The mission to place "a surgical robot in every hospital" faces a stark reality: building a compliant robot today costs too much and takes too long. Roboss eliminates these barriers with MedOS, a revolutionary operating system that commoditizes hardware and shifts the value to software. By running on MedOS, companies can launch a surgical robot 5x cheaper and up to 10x faster without compromising reliability.
MedOS is engineered as a certifiable operating system for surgical robotics and beyond—built from the ground up to streamline regulatory approval while supporting the complex, mixed-criticality workloads of modern medical devices. It uniquely bridges the worlds of research and production by offering native compatibility with the Robot Operating System (ROS), allowing developers to leverage the vast ecosystem of algorithms and libraries while ensuring they deploy on a safe, deterministic, and production-grade platform.
To meet the stringent demands of surgical applications, MedOS integrates the Acontis EC-Master real-time protocol stack. This partnership ensures that while MedOS manages the high-level application logic and safety, Acontis guarantees deterministic, hard real-time communication for precise motion control.
Together, we are not just building another robot; we are enabling a global ecosystem where advanced, affordable robotic-assisted surgery becomes universally accessible.
www.roboss.io