Monitoring and Diagnosis Software and Tools
Acontis is offering several software products for monitoring and diagnosis of EtherCAT networks. This site is showing the features and differences between the products and will help to decide which tool or development kit is needed for which use case.
EC-Engineer is a powerful software tool for Windows and Linux used for configuration, diagnosis, and monitoring of EtherCAT® networks. Using this single tool one can handle all required engineering and diagnosis tasks in a quick and comfortable way. The modern, clear, and very intuitive user interface, which is also rarely using popup dialogs, is crucial for a smooth experience in configuring, diagnosing, and monitoring of EtherCAT® systems.
EC-Lyser helps to figure out issues if the network startup isn't successful, or if the communication is disturbed by bad cables, connectors or Electromagnetic Compatibility (EMC).
EC-Inspector is an easy to use software application for Windows for analyzing, troubleshooting and monitoring EtherCAT networks. The program can be used independently of the standard controller and works with EtherCAT MainDevices (masters) from many manufacturers. EC-Inspector analyzes the complete data traffic between the master and the EtherCAT SubDevices via a TAP (Test Access Point) device inserted after the MainDevice controller. EC-Inspector operates exclusively in passive mode, so there is no risk of unintended changes to the machine or system.
EC-Monitor is a software development kit (SDK) with a library for analyzing the data traffic of an EtherCAT network. The process data (inputs and outputs), the SubDevice states, the SubDevice error counters, and other important EtherCAT data are extracted from the EtherCAT frames and made available to the application via a C programming interface.
System Architectures
Local Diagnosis
The SubDevices are connected directly to the Engineering System (Windows PC or Linux System). The PC is acting as an EtherCAT MainDevice.

Remote Diagnosis (RAS)
The SubDevices are connected to the controller. The diagnosis software connects to the controller via a secondary TCP/IP connection using a proprietary API. This is only supported by EC-Master and the RAS-Server has to active.

Diagnosis with Network TAP
A Network TAP is added to the EtherCAT Network. With this TAP it is possible to monitor EtherCAT traffic with the Engineering System running EC-Inspector. This is supported by numerous master vendors.
Monitoring with Network TAP
The installation of a Test Access Point (TAP) between the controller and the first EtherCAT SubDevice allows passive monitoring of the entire data traffic on the EtherCAT network. The frames are forwarded to the EC-Monitor library via the monitor interface of the TAP and decoded there. A customer application can analyze and further process the determined process data.
Feature Comparison
This table gives a quick overview about the main features of the different software tools and development kits.
|
Features |
|||
|
Configuration: Create Network and MainDevice Information File (ENI File) |
YES |
- |
- |
|
Full-featured Diagnosis Functions: |
YES |
YES |
- |
|
Basic Diagnosis Functions: |
- |
- |
YES |
|
Record EtherCAT communication and offline analyzation of captured EtherCAT communication, e.g., search in Wireshark file for issues |
- |
- |
YES |
|
Record and analyzation of entire process data (lossless). |
- |
- |
YES |
|
Third Party MainDevice Support |
- |
- |
YES |